Close
통합검색
통합검색
통합검색 창 닫기

> Support > Downloads

Downloads

준비중
  • R+ Motion 2.0 (v2.3.1)
  • date : 2016-01-27 | Version : | Views : 11307 Download : 0
R+ Motion 2.0 (v2.3.1) 
 
* Release date : January 15, 2016
* Latest version : v.2.3.1
* Language Support : Korean / English / Italian /Chinese
 
* Precaution before DOWNLOAD
- Due to the recent Windows file regulation change, auto-update may not function properly.
- If you experience any problems after update, please uninstall the previous program then re-install.   

 
* Download
Download Link (31.5MB)
- If you already have R+ Motion installed, please update by using the auto-update function in the program.
- Even if you use this setup file, you MUST uninstall the previous version before proceeding with the installation.  

 
* Update Details  (Updates after v2.2.2)
- Enhanced Windows 10 stability
- Support for serial port filtering Function
- Improved stability for LN-101 and Mini USB (Improved compatibility with the latest FTDI driver)
- Added Italian and Chinese language support
- Fixed motion compile bug
- Mixed minor bugs
 
 
* Link to e-Manual
Please refer to the e-Manual for more information on using the program.
LINK 

* System Requirements
  - OS : Windows XP SP2 or higher
  - Hardware : There won't be any problem operating under H/W released in the last 10 years,
                       but systems with low performance may have difficulties in communication.

 
http://support.robotis.com/ko/images/software/r+motion/r+motion_main.jpg
 
 


  • ROBOTIS INC | 26228 Enterprise Ct. Lake Forest, CA 92630, USA | TEL : +1-949-377-0377 | FAX : +1-949-242-5112