Close
통합검색
통합검색
통합검색 창 닫기

> Support > Troubleshooting

Troubleshooting

Please browse through the list under the related category.
You may find similar topics that may help you to troubleshoot on your own.



  • [ROBOTIS MINI] Programming the ROBOTIS MINI
  • date : 2015-09-05 | Views : 1022
The ROBOTIS MINI can be controlled via PC (Windows or OS X) or smart device (Android or iOS).






To control the MINI via smart device, download the free ROBOTIS MINI app from the Google Play store or
iTunes.





You can program the MINI via the following free software:
Motion 2.0 is a program that will be included in the upcoming RoboPlus 2.0 suite of software. This program allows
you to interact with an on-screen 3D model of your robot create and download motions to your actual robot.



 

Task is a graphical C-based program used to create and download programs to your robot. It is part of the existing
RoboPlus 1.0 suite of software.




 
The ROBOTIS IDE is an Arduino-like IDE designed specifically for programming the ROBOTIS MINI
controller (OpenCM9.04C).* 


 

*Note that users who would like to use RoboPlus after using the ROBOTIS IDE must
restore the controller’s firmware each time they do so.  


 
More information on how to program using Motion 2.0, Task, and the ROBOTIS IDE can be found in the e-manual
under Software Help.



Previous Getting Started with Dynamixel
Next [OpenCM9.04] Recovering OpenCM9.04 Controller Firmware
  • ROBOTIS INC | 26228 Enterprise Ct. Lake Forest, CA 92630, USA | TEL : +1-949-377-0377 | FAX : +1-949-242-5112