...

FAQ

SOFTWARE | Dynamixel MX Series (Protocol v2.0) F/W Recovery

Hit 3,420

본문

The Dynamixel MX series is now compatible with protocol v2.0

The control table for the X series can be adapted to the MX series.
(Improves communication and current control)

Please use the convertible cable to connect the X series and MX series together to control using one source.

Caution :
The default setting for the MX series is protocol v1.0.
The firmware for all MX series (MX-28, MX-64, and MX-106) must be recovered (latest version is 39 released on March 3rd, 2017) to get started.