...
POST No. 21142
PROBLEM WHEN READ FROM CM-5 TO PC A MOTION CREATION
2008-05-21 08:26:00
Hi "bioloiders" ;

Let me ask you an issue!

When I create a motion with "Motion Editor: last version downloadable 1.27"  after save  to flash, when I try to read from PC (in behaviour program: management > robot motion > read option) download banner progress until 90%  where stops and a popup message inform a filed transmision, after repeat several times the result is the same: FAIL!

I addition after write the name of file to save in PC the 3 leds of cm-5 (manage, program, play) BLINK simultaneously , I first click OK and then start to start download an fail I change teh order first press start and then OK (window popup) and aslo fail...

I appreciate so much you help!


SALVE BIOLOID!
Muchas Gracias

RsOLEdom!
2008-05-21 08:26:00
2008-08-28 17:36:00 ROBOTIS
Dear RsOLEdom,Thank you for your kind patience.Our engineers have tested this and found a problem where in certain/special cases the Behavior Control Program does not upload the motion. This has already been solved.I have sent a link to your e-mail. Please check your e-mail.Best Regards,ROBOTIS
2008-08-28 17:36:00
robotis
Reply
웹에디터 시작 웹 에디터 끝