...
POST No. 21591
specifications motor inside
2009-07-01 21:57:00

We will probably use the RX-64 servomotors inside our next robot because it contains a maxon motor. We are currently making a simulation using 20sim. There we need to include the motor specifications to see if the motor produces enough torque-speed. Is it possible to tell which maxon motor is included or give an idea about specifications? This would help us a lot. Because without this information it is very difficult to make the simulation right.

2009-07-01 21:57:00
2009-07-03 10:00:00 ROBOTIS
Dear BramVDB, Unfortunately, we are unable to disclose information on the maxon motor. I apologize for the inconvenience and for not being able to assist you with this. ROBOTIS
2009-07-03 10:00:00
robotis
Reply
웹에디터 시작 웹 에디터 끝