...
POST No. 21623
About the ZIG2Serial Manual
2009-07-21 20:51:00

Sample codes are great, but the manual is bad.

Lots of pictures do not show up.


hope you can release a new ZIG2Serial Manual.


Thanks!

2009-07-21 20:51:00
2009-07-22 13:10:00 Xhacker
Thank you for your quick reply, hope you can release the new manual asap (hope that more English, less Korean).an additional question:the zig2serial should be der are two black things (in the red circle).but my zig2serial has no: so what should i do?Thanks!
2009-07-22 13:10:00
Edit Delete
2009-07-22 13:26:00 ROBOTIS
Dear Xhacker, Please note that the first picture is a picture with the ZIG-100 and Zig2serial connecrted. Also, the circled black part is the OLD version of the ZIG-100. The one you have is the current version. About the manual. I am unable to find any Korean in the current manual. Which Korean are you talking about? Any reply would be appreciated. ROBOTIS
2009-07-22 13:26:00
robotis
2009-08-13 09:39:00 ROBOTIS
Dear Gorbag, Thank you for your comment. Can you please send/attached a screen shot of the page with the problem? We can not seem to find the problem on our end. It would help us greatly in getting the problem solved. ROBOTIS
comment
2009-07-23 08:46:00
Why you want to keep the cm-5 firmware? It just provide two functions: run Behavior Control Program and call motion pages. (may be also charge).The C can replace Behavior Control Program well, and you can write a function youself to replace motion pages (maybe a array to save positions), charge program is easy to write too.So why?Xhacker
2009-07-23 08:46:00
2009-08-04 11:07:00
Hi Mauricio,

ROBOTIS does not currently have plans on developing a SDK for users to make their software.

Kayla
2009-08-04 11:07:00
2009-08-13 09:39:00
robotis
Reply
웹에디터 시작 웹 에디터 끝