...
POST No. 21650
problem with robot terminal
2009-07-30 15:24:00

hello robotis.
 I  was making a motion with robot terminal in page "3" .but when I
play that page,the first step (step 0) is slower than other
steps,whereas all speeds are "32".
could you help me to fix this problem?

 

thank you.


2009-07-30 15:24:00
2009-07-30 15:58:00 ROBOTIS
Dear Khashi, What version is the CM-5 you have? The current released version is 1.15v so if you have one that is before this it may be a problem. Please check whether there is a pause time. How is it in other pages? Can you please send us a capture of the page with the problem. It should help us a great deal. Another option you can do is, get a motion initializing file and erase all the motions and start again.Attached is the ROM file. ROBOTIS
2009-07-30 15:58:00
robotis
Reply
웹에디터 시작 웹 에디터 끝