...
POST No. 21735
some quetions about the rx-28
2009-11-11 20:13:00

Hello,

I've got a few questions about my rx-28.

1 From the manual, I get that, if the Action command is delivered without the reg_write command, it can produce an error bit through adress 0x11 of the control table. Does it mean that continuous delivering of action commands to rx-28 without a reg_write command will do any harm to rx-28? Or it just doesn't produce any influence?

2 The recommanded voltage applied to rx-28 is 12~16V, while actually I use a 16.8V voltage to produce a larger torque. Will it do harm to rx-28?

3 The attached is the connection of rx-28 in my robot system, is there any problem? I find that with a same program, some rx-28 can always be read successfully, while others can only be read sometimes. Does it have anything to do with the connection?

Tangk you!

Sincerely

Vickyzer

2009-11-11 20:13:00
Reply
웹에디터 시작 웹 에디터 끝