...
POST No. 21747
question about the torque
2009-11-24 11:26:00

?Hi,

?I'd like to know what are these parameters used for .

P_MAX_TORQUE_L

P_MAX_TORQUE_H

P_TORQUE_LIMIT_L

P_TORQUE_LIMIT_H

and what's the difference between "max torque" and "torque limit" ? in the manual , the explanation are the same.

 

Thanks a lot.

Nero

2009-11-24 11:26:00
2010-08-31 18:02:00 taufik
HI,How to achieve a high torque with low speed of AX 12 in endless turn. I found that a high speed, the torque is high, as compared to the low speed the torque is really small. I had set the max torque and torque limit at 1023. I assume the speed control is using the voltage proportional, but not PWM.. If this is the problem, how can I use a PWM method to control the speed in endless turn.regards,taufik
2010-08-31 18:02:00
Edit Delete
Reply
웹에디터 시작 웹 에디터 끝