...
POST No. 22010
[ZIGBEE] communication inquiry
2010-04-20 03:43:00

Hi,

“the problem im having is that when i insert the wireless chip into the remote control it appears to be fine eg. powers up and lights flash.

 i plugged the zigbee adapter into my controller it lights up and the leds on the controller appear to be recieving and sending data but nothing works.. im obviously missing something

im still new to this robot so bare with me

i appologize for the newbee question..

thanks in advance..”

2010-04-20 03:43:00
2010-04-21 15:02:00 ROBOTIS
Dear Carlos, It seems that your wireless communication is working right, if the led of controller lit up when you send data. Please check if a serial cable is connected between the robot controller and PC. When a serial cable is connected, it is not possible to use the wireless communication. If not, the second possibility is the controller. Please download the motion and task program below and play your robot. http://support.robotis.com/en/product/bioloid/premiumkit/download/bioloid_premium_demo.htm Thanks. ROBOTIS
2010-04-21 15:02:00
Edit Delete
Reply
웹에디터 시작 웹 에디터 끝