...
POST No. 2406655
Some Further Ardunio IDE Questions for OpenCM 9.0.4 connection
2018-01-03 22:58:18 fatihirim

Hello


By using USB cable, I was able to connect an XL-320 to Ardunio IDE (running on Ubuntu) through Open CM 9.0.4. I was also able to run the attached sketch (xl-deneme.ino).


However, when I tried to run the sketch for AX12 (I did modify relevant parts of the code like control table references etc.) it did not work. I used Open CM Expansion Board on top of Open CM for connecting AX12 to Ardunio IDE. I can`t get the connection established. (I get "There is no status packet" error)


I attach the sketch for XL-320 and also the sketch for AX-12 (ax-deneme.ino). Could you please try my sketches and check where the problem is??


PS: In my sketch for ax12, I tried DEVICENAME to be "3" and also tried "/dev/ttyACM0". But neither worked. Which one should I normally use? What is the difference between using the DEVICENAME (i.e. port) as 1,2,3, or /dev/ttyACM0?


Thanks in advance!

2018-01-03 22:58:18
fatihirim
2018-01-04 11:18:04 Will Son

Hello,


In order to use Dynamixel connected to 485 EXP board, you should use DEVICENAME "3" which is correct in your source code.

AX series use 2 byte Goal Position and Present Position data, therefore, you need to use the following read/write functions.


// Write goal position

dxl_comm_result = packetHandler->write2ByteTxRx(portHandler, DXL_ID, ADDR_PRO_GOAL_POSITION, dxl_goal_position[index], &dxl_error);


// Read present position

dxl_comm_result = packetHandler->read2ByteTxRx(portHandler, DXL_ID, ADDR_PRO_PRESENT_POSITION, (uint16_t*)&dxl_present_position, &dxl_error);

2018-01-04 11:18:04
willson
Reply
웹에디터 시작 웹 에디터 끝