...
POST No. 2406715
Forum: More control on order of threads...
2018-03-04 02:08:30 kurteck

Was wondering, on most forums that I am on, you have some control on things like the order in which the threads are shown.


Example on most forums, the order I typically see things is in the order of the time of the last posting to a thread.  So for example if I posted a thread about something like: support on other boards and several days later some one posts a reply, I may not notice it as it may be on the 2nd or 3rd page of postings.


Also on most forums, the threads show differently for those on which I have unread postings.


So wondering if this forum has these capabilities and I am somehow missing it?  Or if not, it would be great to add it as a wish list.


Kurt

2018-03-04 02:08:30
kurteck
2018-03-05 15:44:59 Will Son

Hello Kurt,


Yes, I agree with the need of those cool features.

Although this is named as "Forum", it is not like the latest forum platforms such as discourse.

We're planning to move onto those platforms in the near future, but haven't decided when will it be.

Appreciate for your suggestions :)

2018-03-05 15:44:59
willson
Reply
웹에디터 시작 웹 에디터 끝