...
POST No. 2406716
[USB2Dynamixel][XL430-W250-T] Issue: cannot update Dynamixel on R+ Manager #164
2018-03-05 09:57:17 redragonfly3

https://github.com/ROBOTIS-GIT/DynamixelSDK/issues/164

We have recently purchased several Dynamixel XL430-W250-T to build a Turtlebot 3. We have installed R+ Manager 2.0 to update the firmware with the desired baudrate and ID. However, we haven't managed to set the Dynamixels.

We are connecting the Dynamixel to a computer via USB2Dynamixel. After we select "Update & Test" on R+ Manager 2.0 the motor is detected correctly. However, afterwards the communication status of RX is shown as "corrupt" and we get a "CRC error". We haven't been able to change the baud rate or the ID. The TX channel blinks and is sometimes shown as green and sometimes as grey.

capture r dynamixel issue

When we try to do the firmware recovery the installation always fails. Sometimes it fails at 0%, and sometimes at 99.67%. Afterwards we have the problem that the Dynamixel is not even detected anymore, and the red light of the motor does not turn on when we power it.

capture failed installation dynamixel

We would greatly appreciate any help on this matter.

2018-03-05 09:57:17
redragonfly3
2018-03-05 15:47:21 Will Son

Hello,


Could you specify the power source you are using?

XL430 requires DC 12V power supply in order to operate properly.

2018-03-05 15:47:21
willson
2018-03-09 18:07:48 Adrian

Hello,


Thank you for your answer. We are using one of the TTL sockets of the OpenCR to power the motor, could that be the problem?

2018-03-09 18:07:48
Adrian_1
2018-03-12 11:37:53 Will Son

In that case, OpenCR1.0 will also try to respond to the signal from R+Manager and could cause such issue.

Please try to supply power only from OpenCR1.0 by pulling out the Data pin from the cable.

Thank you.

2018-03-12 11:37:53
willson
2018-03-13 19:57:19 Adrian
Thank you, we will do that as soon as possible and update on the result.
2018-03-13 19:57:19
Adrian_1
2018-03-16 02:00:56 Adrian

Just a small note: we won't be able to test the suggested solution until early April, but please do not close this issue due to lack of answers from our side. We will reply back again in a couple of weeks.

comment
2018-03-16 10:19:01 willson
No problem :)
When you come back, please open a new thread as current threads do not send notifications which makes us difficult to follow up or keep track.
Thank you.
2018-03-16 10:19:01
willson
2018-03-16 02:00:56
Adrian_1
Reply
웹에디터 시작 웹 에디터 끝