...
POST No. 2406766
Issue of MX-64R and MX-64AR
2018-04-16 18:12:44 Allie

Hi  Sir, 


Please check the vedio, We checked the gear is ok and communication connect is ok. But the servo can not work.


What is the problem?

2018-04-16 18:12:44
Allie
2018-04-17 02:16:10 Kurt

Sorry, I don't have any of these servos, I mainly have AX servos and now a few XL and XM.  So maybe someone from Robotis might be able to figure something out, but.


My guess is, it would help to have some additional information, like what is not working? 


That is do you have it hooked up to some controller? Which one, controlled by ??? You are trying to get it to do???  What is it actually doing?

2018-04-17 02:16:10
kurteck
2018-04-17 09:46:23 Will Son

Hello Allie,


According to your video(qq视频20180416170104.mp4), it seems the motor is not in a good condition.

Or check if the power supply is providing enough current and cable is fine.

You might need to repair the motor 


The second video with Dynamixel Wizard, if you set both CW/CCW Limit to '0', Dynamixel will operate as Wheel Mode.

Wheel mode doesn't accept position command therefore you cannot control the angle. If you wish to control the angle, you have to set as Joint Mode

Please see the eManual. Click on the "Google" button to see language translation option

 


If the Dynamixel in the second video is the identical Dynamixel with the first video, you need to repair the motor as it shows Overload Error in bit 5 after sending an instruction.

This seems to be either the motor core draws too much current due to a malfunction or the damaged gear.

Thank you.

2018-04-17 09:46:23
willson
Reply
웹에디터 시작 웹 에디터 끝