...
POST No. 2406851
Is it possible to reset the Multi Turn mode count in the X Series motors without updating to the new firmware(v42)?
2018-06-08 14:33:35 jmoon

Could we set the goal position value to 0 in Extended Position Control Mode (Multi-turn) without making the motor turn in the opposite direction?

OR alternatively, is it possible to read the present position or have accuracy of position while in wheel mode (Velocity Control Mode)?

2018-06-08 14:33:35
jmoon
2018-06-11 15:12:35 Will Son

Hello,


Resetting the turn count is newly added in the latest firmware, therefore, it cannot be used in the previous firmware version.

However, you can read Present Position while operating with Velocity Control Mode.

The Present Position range for X series is -2,147,483,648 ~ 2,147,483,647 which is 524,288 revolution for each direction.

Our TurtleBot3 is using this value(left and right wheels are set as Velocity control mode) for estimating its present location as well.

If your application is unlikely to exceed above range, you can definitely  use above 4byte position value.

Thank you.

2018-06-11 15:12:35
willson
Reply
웹에디터 시작 웹 에디터 끝