...
POST No. 2406854
Several issues with OP3
2018-06-12 11:47:31 super_radioman

Q1. I updated the latest firmware, and then executed “bringup”; however, it still did not work.

 

According to the link: http://emanual.robotis.com/docs/en/platform/op3/tutorials/#bringup


 

Still failed to find out “op3_bringup”


 


 

 

Q2. When I was executing “Ball_detector”, the error message came out, as the following picture.



 

 

 

Q3. It was not stable while the demo program, face recognition, was executing.

Should I modify the parameters as the following picture?

 
 


2018-06-12 11:47:31
super_radioman
2018-06-12 13:35:12 Will Son

Hello, 

The identical issue has been posted by cyberobotics in below postings.


Q1 : http://en.robotis.com/service/forum_view.php?bbs_no=2406852&page=1&save_sca=&sca=&save_stx=&stx=&sfl=


Q2 : This is because of the ROS version difference. You can disregard this message as it will not affect to the functionality.


Q3 : OP3 use open source face detection software by phil333. You can get more information from the original repository(https://github.com/phil333/face_detection).

Since OP3 does not use depth camera nor compressed image, changing compressed or compressed depth options will not affect to the performance.


Thank you.

2018-06-12 13:35:12
willson
Reply
웹에디터 시작 웹 에디터 끝