...
POST No. 2406992
MX-106T Backlash
2018-10-08 22:09:35 scott_robosavvy

Hi 


I have a customer with 2 MX-106T servos and 1 has more backlash than the other.  See video attached.


Is there any way to solve this via the customer? This causes quite an issue when using them together.


Thank you.

Scott

2018-10-08 22:09:35
scott_robosavvy
2018-10-12 17:14:12 Will Son

Hello Scott,


Due to the characteristics of the spur gear, there's a backlash and its angle can be bigger as metal gear gets worn out.

If the customer has been using the MX-106T, replacing to new gear set could reduce the backlash gap.

Thank you.

2018-10-12 17:14:12
willson
2018-10-12 17:53:48 Scott Heppell

HI Will


Thank you for your response.  I will see if this is the case.


Scott

2018-10-12 17:53:48
scott_robosavvy
2018-10-12 19:43:24 Scott Heppell

Hi Will


Both of these servos have never been used so this backlash is just from taking them out of the box and inspecting them.


What would be the process of getting this looked in to? 


Thanks

Scott

2018-10-12 19:43:24
scott_robosavvy
2018-10-15 09:36:26 Will Son

Hi Scott,


If the customer's application is very sensitive to the actuator's backlash, it is recommended to use Pro series which use cycloid gear that reduces backlash by 80% than MX series.

The backlash with spur gears is inevitable due to its mechanism, so we have a specific standard for the quality.

However, if the customer requests RMA, we'll take a look at it and see if it can be reduced.


Thank you.

2018-10-15 09:36:26
willson
2018-10-15 17:36:09 Scott Heppell

HI Will


Thanks for your response.  I will pass it along.


Scott

2018-10-15 17:36:09
scott_robosavvy
2018-10-16 01:03:18 Scott Heppell

Hi Will


The customer is strapped for time so they are going to try to use them as is.  But he may be back if he cannot overcome the current backlash issue.


Thank you for your assistance.


If an RMA is needed I should contact John correct? Or can I attach the form here?


Thanks.

Scott

comment
2018-10-16 15:42:39 willson
Scott,

You can always contact John for RMA.
Thank you.
2018-10-16 15:42:39
willson
2018-10-16 01:03:18
scott_robosavvy
Reply
웹에디터 시작 웹 에디터 끝