...
POST No. 2407085
R+ Motion error (The network location cannot be reached. For information about network troubleshooting. see Windows Help)
2018-11-07 07:05:13 Almohsin

i have used the R+ Motion to edit motion. i used the 3D robot  as an interface to control the actual robot(Darwin-Mini), but when i try to connect the actual robot to the 3D robot, i have got this error (The network location cannot be reached. For information about network troubleshooting. see Windows Help). I tried to change my network sitting from public to private, and finally the actual robot connect with the 3D robot successfully.  However, when i shut the laptop down and back again i got the same error again, even i do not change the previous network sitting it still private as before.

Here are the steps i have done :

1- Paired the actual robot with the laptop via the Bluetooth.

2-Add the robot as device on the laptop.

3-Turn the actual robot ON.

4-Press the connect button on the R+ Motion.

5-Choice the serial port COM4 .


Note: windows 10 are used as platform here. 

2018-11-07 07:05:13
Almohsin
2018-11-07 13:34:39 Will Son

Hello Alweh,


I'm sorry for not being able to help you with issues regarding Windows system.

There are similar questions on Windows community so you might want to try them.

Thank you.

2018-11-07 13:34:39
willson
2018-11-12 10:02:09 Will Son

Hi Alweh,


Could you specify the Bluetooth module you are using?

Is it BT-210?


=========Edited===========

This is identified as a BT-210 compatibility issue with the Windows 10 update.

Please request RMA to your local reseller for BT-210 firmware update.

Thank you.

2018-11-12 10:02:09
willson
Reply
웹에디터 시작 웹 에디터 끝