...
POST No. 2407340
Problems to manage DXL Pro with U2D2
2019-03-12 20:23:40 imarvi2

Hi,


I try to manage DXL Pro with U2D2 but I cannot have accesss to most of the control table (see enclosed file for details).


I have cheched thay DXL is properly powered and that serial port to whih U2D2 is connected is set to 9600 bds and latency of 1.


Could you plesse help?


Thanks un advance,


Iván M.

2019-03-12 20:23:40
imarvi2
2019-03-13 10:43:32 Will Son

Hi,


You are using DYANAMIXEL Wizard 1.0 which only supports Protocol 1.0.

Since your DYNAMIXEL PRO is using Protocol 2.0, you should use R+Manager 2.0 or DYNAMIXEL Wizard 2.0.

I'd recommend to use DYNAMIXEL Wizard 2.0.

http://emanual.robotis.com/docs/en/software/dynamixel/dynamixel_wizard2/

Thank you.

2019-03-13 10:43:32
willson
2019-03-14 18:50:59 ivan martinez

It works! Thanks, Iván

2019-03-14 18:50:59
imarvi2
Reply
웹에디터 시작 웹 에디터 끝