...
POST No. 2407476
48 x XL320 long chain
2019-07-08 20:15:03 robotitaly

Hello,

I have a question: is it possible to chain 48 XL320 servos with the standard 100mm cable for a total length of about 3 meters?

Also, any issues connectin 6 x XL320 with a custom 400mm cable for a total length of about 3 meters?

Any potential issue?


Thanks

2019-07-08 20:15:03
robotitaly
2019-07-11 16:28:54 Will Son

Hi,


It is recommended to use less than 10 DYNAMIXEL in a single channel.

Although due to Diasy Chain feature, maximum 253 DYNAMIXEL could be connected under ideal condition.

However, as cables get longer, resistance increases and voltage drops, and digital signal becomes vulnerable to external noises(TTL is way more vulnerable than RS-485).

When using TTL (3pin connector) DYNAMIXELs, it is recommended to use within 1 meter range.

Thank you.

2019-07-11 16:28:54
willson
Reply
웹에디터 시작 웹 에디터 끝