...
POST No. 2407484
Using USB-RS485 bridge
2019-07-11 20:11:20 TomasJ

Hello, I am trying to operate H54 100W using simple https://shop.in-circuit.de/product_info.php?products_id=81 . I know for a fact that it is possible although I would like to have some more insight from you on this. 

Will I be able to do it even if I want to operate more than one such motor.

I also would like to know if it will be possible to use dynamixel wizard 2.0 with device I have and if I can expect some problems, and the only logical choice for me would be to simply buy U2D2.

Thank you.

2019-07-11 20:11:20
TomasJ
2019-07-12 11:29:41 Will Son

Hi,


Thank you for your inquiry.

Although there are many talented engineers who implement various components from multiple brands without a problem, I strongly recommend to use U2D2 with DYNAMIXEL for several reasons.

  1. U2D2 is an official ROBOTIS USB-RS485/TTL converter.
  2. U2D2 supports higher baudrate up to 6Mbit/sec(6Mbps)
  3. If you are operating one or two H54-100-S500-R, U2D2 Power Hub Board will make system harnessing much easier and organized.
  4. U2D2 is tested with DYNAMIXEL Wizard 2.0 and compatible with various features such as graph plotting at 1ms refresh rate(1Khz), packet analyze and self diagnosis.
  5. U2D2 supports up to 253 DYNAMIXELs in a single channel.
Since I do not have any experience on the product, it is very difficult for me to expect the consequence of the combination.
Thank you.
2019-07-12 11:29:41
willson
Reply
웹에디터 시작 웹 에디터 끝