...
POST No. 2407656
FSR problem for op2
2019-11-08 23:08:13 aysegulucar

Hi,


I inserted FSR set to op2. I did not work a command in robot.


I just run linux/projects/fsr    ./ fsr


I received an error as in figure.


What is problem?


Many thanks.




2019-11-08 23:08:13
aysegulucar
2019-11-12 11:22:15 Will Son

Hi,


When you are running tools, you need to kill the demo program that runs at startup.

http://emanual.robotis.com/docs/en/platform/op/development/#tutorial-procedure-6

Please refer to below instruction to terminate the demo program.

http://emanual.robotis.com/docs/en/platform/op/development/#terminate-demo-program

Thank you.

2019-11-12 11:22:15
willson
2019-11-14 23:14:02 aysegul ucar

Thanks for answer. I did it. However I cant see the other figure window (mpjeg stream) .  Why? 


 

2019-11-14 23:14:02
aysegulucar
2019-11-15 09:24:43 Will Son

Hi,

You need to open the internet browser and enter the address below to access the screen.

http://<enter OP2 IP Address here>:8080

For example, http://192.168.123.1:8080 

Thank you.

2019-11-15 09:24:43
willson
2019-11-16 02:39:08 aysegul ucar

Hi,

Thanks. I have new error. version problem as in the attachment at figure.


How can I solve the problem?


Thank you 

2019-11-16 02:39:08
aysegulucar
2019-11-18 22:02:35 aysegul ucar

?

2019-11-18 22:02:35
aysegulucar
2019-11-22 01:49:11 aysegul ucar

?

2019-11-22 01:49:11
aysegulucar
2019-11-22 22:34:19 aysegul ucar

 

2019-11-22 22:34:19
aysegulucar
Reply
웹에디터 시작 웹 에디터 끝