...
POST No. 2407690
Dynamixel MX-28T works but doesn't get recognized on Dynamixel wizard
2019-12-05 00:20:54 abuzaa
Hi there, Hope you are doing well. So, the thing is I use four Dynamixel motors of type MX-28T, each pair used to control a robotic arm , one of the robotic arms is shown in the attached image "Robotic arm set-up". I use USB2dynamixel (COM19) on TTL mode and actually the motors work words are written to them but read doesn't work for all of them, with the set IDs (each has a unique ID). Attached picture of USB2Dynamixel is attached. When i tried to check them on dynamixel wizard, I connect only one motor at a time when I search for the dynamixels, I only found that one of the 4 is recognized and others when connected separately aren't, as shown in "Dynamixel Wizard " attched picture. The LEDs of all 4motors blink normally when power cable is plugged. I tried to update the firmware or even do recovery but still the wizard can't find the motors in the first place. So, does anyone know how I can get the other 3 dynamixels to be recognized on the wizard or what actually might be causing this problem and why words can't be read on Labview, although it write words!? Thank you so much in advance. your help would be appreciated. Some info. : -Used controller and program: Myrio, Labview 2016 -OS: Windows 7 -Protocol used for dynamixels in Labview: protocol 01 - Each two dynamixel motors are connected in series Attached images: shorturl.at/imDM7
2019-12-05 00:20:54
abuzaa
2019-12-05 03:35:17 Will Son

Hi,


You might want to try searching them with DYNAMIXEL Wizard 2.0.

If writing to DYNAMIXEL works, but reading from them fails, it could be caused by failure in USB2Dynamixel.

Thank you.

2019-12-05 03:35:17
willson
Reply
웹에디터 시작 웹 에디터 끝