...
POST No. 2407737
op3_action_editon.launch不能运行,别的程序都能运行,请问怎么什么原因,怎么解决呢。
2020-02-06 21:25:14 geyyong

robotis@robotis-op3 ~ $ roslaunch op3_action_editor op3_action_editon.launch

[op3_action_editon.launch] is neither a launch file in package [op3_action_editor] nor is [op3_action_editor] a launch file name

The traceback for the exception was written to the log file

2020-02-06 21:25:14
geyyong
2020-02-10 11:21:14 Will Son

Hi,


Please note below correct command for launching action editor from OP3 eManual.

$ roslaunch op3_action_editor op3_action_editor.launch


Please also note that other programs such as op3_manager, op3_offset_tuner, op3_walking_tuner should not be running when executing the action editor.

In order to terminate the demo program that is running based on op3_manager, you can enter below command in the OP3 terminal.

$ sudo service OP3-demo stop


Thank you.

comment
2020-02-11 07:59:23 geyyong
您好,
$ roslaunch op3_action_editor op3_action_editor.launch 此条命令因为试了好多次,所以不可能输入错误,可见图上并没有错误,
$ sudo service OP3-demo stop 此条命令在运行$ roslaunch op3_action_editor op3_action_editor.launch之前,之后都有尝试运行过,结果都一样。
谢谢
2020-02-11 07:59:23
geyyong
2020-02-11 08:40:27 geyyong
另还想问一下op3_action_editor.launch中

motion_4095.bin文件可以用别的软件打开吗,更多的动作文件可以在哪里下载的到吗?
谢谢
2020-02-11 08:40:27
geyyong
2020-02-11 09:07:51 geyyong
RoboPlus Motion Editor,请问可以编辑OP3动作吗?
2020-02-11 09:07:51
geyyong
2020-02-10 11:21:14
willson
2020-02-11 08:00:39 huang


 

2020-02-11 08:00:39
geyyong
2020-02-19 09:55:19 Will Son

Hi,


Please make sure to enter the correct launch file name.

It seems like you are using "op3_action_edition.launch", but this has to be revised to "op3_action_editor.launch".

Using [Tab] key on the keyboard will enable autocomplete the command or file name in linux that helps to avoid any typo.

Thank you.

2020-02-19 09:55:19
willson
Reply
웹에디터 시작 웹 에디터 끝