...
POST No. 2407792
ROS dynamixel_workbench_controllers errors
2020-03-27 01:32:09 jack94

I am having trouble using the ROS dynamixel_workbench_controllers package with OpenCR1.0 and two XL430-W250 motors.


I have successfully run the o_Find_Dynamixels arduino sketch and changed motor IDs so it outputs:


 

However, when I try to run find_dynamixels on the ROS workbench package it doesn't detect anything:



Also the dynamixels_controllers.launch file doesn't seem to work, giving me error messages:


I edited the config/basic.yaml file to be:

pan:

  ID: 1

  Return_Delay_Time: 0

tilt:

  ID: 2

  Return_Delay_Time: 0


I also edited the launch file to have default baud rate of 1000000 and usb port is /dev/ttyACM0


Can you please help me figure out why this isn't working?










2020-03-27 01:32:09
jack94
Reply
웹에디터 시작 웹 에디터 끝