...
POST No. 2407937
XM430-W210-T with dynamixel shield not working
2020-08-25 02:34:35 Mohana

Hi,

I'm using  Dynamixel XM430-W210-T with Dynamixel Shield (in arduino IDE). But still I face issues with the motor functioning, like no response from the servo at all (only 'led' on and off from the library example code is working, nothing else). In the serial port of terminal I see only garbage values. I'm puzzled what could be the problem? Could there be any problem with the motor? Is it possible to fix it and make it work again? 


Thank you in advance.

2020-08-25 02:34:35
Mohana
2020-08-25 15:22:26 Will Son

Hi,


You might want to read below thread regarding the Arduino serial port especially if you are using Arduino Uno or Mega.

http://en.robotis.com/service/forum_view.php?bbs_no=2407511&page=2&save_sca=&sca=&save_stx=shield&stx=shield&sfl=wr_subject||wr_content

Thank you.

2020-08-25 15:22:26
willson
Reply
웹에디터 시작 웹 에디터 끝