...
POST No. 2407959
AX12a sideway load
2020-10-15 17:01:46 rick10

Hello everyone,

Do any of you knows what is the maximum load that AX12a's axis can undertake ?

Thanks for the help !

2020-10-15 17:01:46
rick10
2020-10-20 16:08:54 Will Son

Hi,


According to the eManual specification of AX-12A, the stall torque is defined as 1.5Nm.

However, please see the note below since this torque does not represent continuous operational torque.

NOTE : Stall torque is the maximum instantaneous and static torque. Stable motions are possible with robots designed for loads with 1/5 or less of the stall torque. 

Thank you.


2020-10-20 16:08:54
willson
Reply
웹에디터 시작 웹 에디터 끝