...
POST No. 2408087
ROBOTIS OP3 NUCi37th crash
2021-10-20 12:34:38 happy170215

Hi All


Recently, when using OP3-NUC (7th i3), it often crashes (just turned on or used for a period of time), and the problem still does not improve after recovery. Which aspect may cause problems and how to solve them?


thanks

2021-10-20 12:34:38
happy170215
2021-10-22 00:59:30 Will Son

Hi


Depending on the symptom when the system crashes, there could be several possible scenarios.

If the system crashes even after the system recovery, it could be related to the hardware components such as RAM or SSD.

Do you get any error messages when it crashes?

comment
2021-10-26 12:59:56 happy170215
It's didn't show any error messages, just mouse can't move and I need to hold the power button a few seconds to shutdown it.
2021-10-26 12:59:56
happy170215
2021-11-03 11:41:06 willson
I think it could be the issue of RAM or SSD if the system stalls in the middle.
Is the symptom occurs with a specific sequence?
If you can provide the steps to reproduce the symptom, it would be useful to figure out the issue.
Thanks.
2021-11-03 11:41:06
willson
2021-11-04 16:29:39 happy170215
I'm not sure, but it's often happened when I open terminal through connect OP3 via VNC in wifi.
2021-11-04 16:29:39
happy170215
2021-10-22 00:59:30
willson
Reply
웹에디터 시작 웹 에디터 끝