...
POST No. 2408094
Help! Motion example error max e2
2021-11-22 04:57:21 Hagen02
Hello, I have problems with the example movements of the max E2, with the max E1 everything is fine I want to do a demonstration and I cannot load erratic movements
2021-11-22 04:57:21
Hagen02
2021-11-22 14:48:04 rjtp5670

Hi Hagen, 


1. If your software is behind the latest, you need to update it. 


2. Looking at the video, It seems that the decimal point is missing in your motion file (mtn3) and it causes the very huge joint movement (i.e, 65.365 > 65365).


Personally assuming that this is bug for only Turkey now. (What's your country? And where did you download R+Task 3.0 and how did you run the motion file?)


3. Try a different motion file by downloading  01_ENG2_Max_E2_MO.mtn3   and load the file in the R+Task 3.0. See how to open project


4. For more, contact support@robotis.com



2021-11-22 14:48:04
davidpark
2021-11-22 20:50:31 Efraín González Paez

hello! Thanks for answering. I'm from Chile. r + task download it from this page. update r + task I opened the file as you indicated, but the same bug appears, the dots between numbers do not appear as you indicated

2021-11-22 20:50:31
Hagen02
2021-11-22 21:29:48 Efraín González Paez

In the mobile application the same thing happens with the same file of movements

2021-11-22 21:29:48
Hagen02
2021-11-22 21:30:12 Efraín González Paez


 

2021-11-22 21:30:12
Hagen02
Reply
웹에디터 시작 웹 에디터 끝