...
POST No. 2408095
Wrong current reading on XM430-W350-T
2021-11-23 23:03:06 Matheus

Hi, I've just acquired a Dynamixel XM430-W350-T servo, and after a couple days working with it I realized that the current readings from the servo (read using Wizard 2.0) are off in comparison to the power supply readings. I have double checked it with a multimeter and the values from the servo are about twice the values from the power supply and multimeter.


I was wondering if there some adjustments or settings I should change to adjust the readings or the servo came with malfunction and there is no way to fix the issue? 


Thank you in advance.

2021-11-23 23:03:06
Matheus
2021-11-25 10:55:32 Will Son

Hi,


The current readings from the DYNAMIXEL control table is different from the current supplied from the external power supply.

DYNAMIXEL reads the actual current flows on the coil of the core motor, while your power supply reads the current consumed in the entire module.

Thank you.

2021-11-25 10:55:32
willson
Reply
웹에디터 시작 웹 에디터 끝