...
POST No. 2408130
How pos profile transmit to position controller in MX-64
2022-06-01 22:18:31 shanghairob

Hi, 


could you help explain how the trajectory profile transmit to the position controller?


as my understand, it the pos trajectory tooks 0.6s,  every 0.1s, the pos will transmit to position controller( 0.1s(pos1) 0.2s(pos2)...and so on)


is it a correct understanding? 


one of my problem is If MX-64 attached a heavy link, how could guarantee the trajectory will be followed by MX-64?


thanks a lot!

2022-06-01 22:18:31
shanghairob
2022-06-13 17:32:01 Will Son

Hi,


I'm sorry about the delayed response.

Please use the ROBOTIS community as there are more useful information and active discussions.


Yes, the Time-based profile will create a trajectory over a given time while referring the present position internally.

In case of attaching a heavy load at the horn, you might need to adjust the PID gains properly so that it can follow the trajectory.


Thank you.

2022-06-13 17:32:01
willson
2022-06-23 22:38:22 por1122

pg slot auto สล็อต ฝากถอนออโต้ ไม่มีขั้นต่ำ ฟรีเครดิต ทดลองเล่นฟรี พีจีสล็อต รวดเร็ว ปลอดภัย รองรับ ทรูมันนี่ ทรูวอลเล็ท ลิขสิทธิ์แท้ ระบบ AUTO มีดีที่ มีระบบเสถียร และความรวดเร็ว 

2022-06-23 22:38:22
por1122
Reply
웹에디터 시작 웹 에디터 끝