...
Item Information

BT-210

상품 선택옵션 0 개, 추가옵션 0 개

SKU 902-0076-000
Manufacturer ROBOTIS
Origin KOREA
Currency USD
Price $ 32.90

선택된 옵션

  • Quantity

상품 기본설명

Features

BT-210 is a device that enables serial communication (UART) via Bluetooth communication.

BT-210 has a case that protects the circuits and a connector-type cable to connect the device onto the robot.

Package Components
BT-210 (120mm cable included)1
H/W Specification
Weight4.51g
Dimensions18mm x 30mm x 9.1mm
Bluetooth SpecificationsBluetooth Specification 2.1 Support
Effective Communication Range10m
Bandwidth Frequency2.4 GHz ISM Band
BandwidthMAX 250kbps
Default Baud Rate57600bps
Sensitivity-81dBm (Typical)
Transmit Power4dBm (Typical)
Bluetooth Profile SupportedSPP (Serial Port Profile)
Operational Voltage3.3V
Consumed Current48mA (Max)
Operating Temperature-40C ~ 85C
Baud rate Range1,200bps ~ 400,000bps
AntennaChip Antenna
InterfaceUART (3.3V Level)
Conducted Net Power-6 ~ 4dBm(Class 2)
Compatible Products

Controller : CM-530 (wireless control, wireless downloading)

CM-510, CM-700 (wireless control / requires firmware update)

Caution

Only contains 1 slave module for assembling onto the robot.

The default pin code is 0000.

Please refer to the e-Manual for more information on how to change the code.

Can be used to control the robot with devices that support Bluetooth communication.


* NOT Compatible with :

Remote controller : RC-100, RC-100A

Controllers : CM-100, CM-5, CM-2+

1. All international orders are processed via DHL from KOREA (not USA) unless otherwise requested.
2. Orders are normally processed within a 2 week time period. A lead time is applicable for certain items. (Normally ships out within 3 working days when in stock).
3. If multiple orders are placed on the same day, they will be shipped in the same package, unless requested to ship separately by order. If an error is discovered in your order that requires change or cancellation, please contact us immediately. We will not be held responsible for any costs that may arise due to your negligence.
4. Please note that destination charges (import tax, customs duty, etc.) are not included in the shipping charges. We will not be able to calculate or pre-pay this fee for you.
5. If an order is placed and the payment is not settled within 14 days, it will automatically be cancelled. If necessary, please re-place the order and make the payment in a timely manner.
6. We recommend you to insure your orders to avoid lost or damaged shipments which is 1% from the total invoice value. We will not be held responsible for lost or damaged shipments.
1. If you are not completely satisfied with your order you may return it within 14 days from your shipment date for an exchange or refund. However, all non-defective products must be in their original packaging, and un-opened new condition. We will not be held responsible for return shipping charges.
All returns must go through the RMA process prior to being sent back to us.
Please note, we will not make any exchanges or repair unless WE HAVE ISSUED YOU AN RMA#.
Please check warranty.
2. Returned packages must include an RMA number on the outside of the package, as well as a copy of your printed invoice.
If you do not have your invoice, please include your name, address and phone number, so we may contact you regarding any questions we may have.
We have the right to refuse your shipment if we have not issued a RMA nubmer.
3. All returned items must be in there original package state. We are not responsible for damage to the print-head or circuitry as a result of improper handling, storage, or misuse.
When removing protective tape and devices please be sure not to damage these areas.
4. Requests for replacement or refunds will not be granted until your returned packages have been received.
5. Please allow up to 14 business days to process your refund from the time it reaches our warehouse, if you need an immediate replacement, we recommend that you place a new order and request a refund of the original order separately. We will not be held responsible for cancellatioin fees.
6. When returning any items, please confirm return address and keep note of the tracking number to avoid losing shipments.
We will not be held responsible for lost items.
7. We reserve the right to deny credit or replacements and charge the customer for parts and labor if the product returned are deemed satisfactory or non-defective.
8. We are not responsible for customer shipping costs to return non-defective or incorrectly ordered products.
9. Customers must obtain a Return Material Authorization('RMA') number by contacting Customer Service at contactus2@robotis.com. Returned products should be informed in advance before being returned.