...
Item Information

CM-150

SKU 902-0103-000
Manufacturer ROBOTIS
Origin KOREA
Currency USD
Price $ 59.60

Out of stock.

This product is temporarily out of stock due to the global supply chain issue.

상품 기본설명

Features

-CM-150 controller is used with ROBOTIS DREAM.

-Various DREAM parts (geared motor, servo motor, touch sensor, LED module, IR sensor, etc.) can be connected to CM-150.

-RoboPlus Manager (Version 1.0.30.0 or higher) can be used for firmware recovery.

-RoboPlus Task (Version 1.1.0.0 or higher) can be used to write task code that is downloaded onto CM-150.

-A mini USB cable or an LN-101 can be used to connect CM-150 with a PC to download programs.

-The m.Task app for mobile devices can be used to download programs using a wireless module.

-BT-210 / BT-110A / ZIG-110A wireless modules can be connected to CM-150 for wireless downloading.

-CM-150 controller does NOT support RoboPlus Motion.

Package Components
CM-150

1

*Download Cable is not included.

H/W Specifications

Weight

21g

CPU

ARM Cortex STM32L151C8

Voltage Supply

Range : 3.2V ~ 4.2V

Recommended : 3.7V (Li-ion Battery x 1)

Current Consumption

Standby : 50mA

Running : 70mA

Max : 300mA

Operation Temperature

-5℃~70℃

Internal I/O components

IR sensor (measure distance) x 3

Mic (Sound sensor) x 1

Buzzer x 1

External I/O components

4-pin comunication (wireless control & download) x 1

Micro USB port (connect to PC) x 1

Motor port (for reduction motor) x 2

Multi-usage port(sensor and outputs) x 2

Compatible Products

Sensor : IR Sensor, Touch Sensor, Color Sensor, Magnetic Sensor

Wireless Communication : IR Receiver, ZIG-110A, BT-110A, BT-210

Etc. : Servo Motor, Geared Motor, LED Module

Caution

The CM-150 can NOT replace the CM-100A. 

Embedded programs are not provided, and does not support other software other than RoboPlus. 

1. All international orders are processed via DHL from KOREA (not USA) unless otherwise requested.
2. Orders are normally processed within a 2 week time period. A lead time is applicable for certain items. (Normally ships out within 3 working days when in stock).
3. If multiple orders are placed on the same day, they will be shipped in the same package, unless requested to ship separately by order. If an error is discovered in your order that requires change or cancellation, please contact us immediately. We will not be held responsible for any costs that may arise due to your negligence.
4. Please note that destination charges (import tax, customs duty, etc.) are not included in the shipping charges. We will not be able to calculate or pre-pay this fee for you.
5. If an order is placed and the payment is not settled within 14 days, it will automatically be cancelled. If necessary, please re-place the order and make the payment in a timely manner.
6. We recommend you to insure your orders to avoid lost or damaged shipments which is 1% from the total invoice value. We will not be held responsible for lost or damaged shipments.
1. If you are not completely satisfied with your order you may return it within 14 days from your shipment date for an exchange or refund. However, all non-defective products must be in their original packaging, and un-opened new condition. We will not be held responsible for return shipping charges.
All returns must go through the RMA process prior to being sent back to us.
Please note, we will not make any exchanges or repair unless WE HAVE ISSUED YOU AN RMA#.
Please check warranty.
2. Returned packages must include an RMA number on the outside of the package, as well as a copy of your printed invoice.
If you do not have your invoice, please include your name, address and phone number, so we may contact you regarding any questions we may have.
We have the right to refuse your shipment if we have not issued a RMA nubmer.
3. All returned items must be in there original package state. We are not responsible for damage to the print-head or circuitry as a result of improper handling, storage, or misuse.
When removing protective tape and devices please be sure not to damage these areas.
4. Requests for replacement or refunds will not be granted until your returned packages have been received.
5. Please allow up to 14 business days to process your refund from the time it reaches our warehouse, if you need an immediate replacement, we recommend that you place a new order and request a refund of the original order separately. We will not be held responsible for cancellatioin fees.
6. When returning any items, please confirm return address and keep note of the tracking number to avoid losing shipments.
We will not be held responsible for lost items.
7. We reserve the right to deny credit or replacements and charge the customer for parts and labor if the product returned are deemed satisfactory or non-defective.
8. We are not responsible for customer shipping costs to return non-defective or incorrectly ordered products.
9. Customers must obtain a Return Material Authorization('RMA') number by contacting Customer Service at contactus2@robotis.com. Returned products should be informed in advance before being returned.