...
Item Information

LIPO Battery 11.1V 1000mAh LB-010

상품 선택옵션 0 개, 추가옵션 0 개

SKU 903-0143-000
Manufacturer YUNTONG POWER CO LTD
Origin CHINA
Currency USD
Price $ 23.90

선택된 옵션

  • Quantity
Features

This LiPo battery is intended for robots. 

PCM is incorporated to protect the battery from overcharge, discharge, and excessive current.

Can be recharged with LBC-010 Battery Charger.

Package Components
LIPO 11.1V Battery LB-0101
Battery Cover-T1
FP04-F601
Battery Extension Cable1

* Battery Charger (LBC-010) sold separately

H/W Specifications
Weight83g
Size70mm x 35mm x 15mm
Voltage11.1V
Capacity1000mAh
Discharge Rate10C
Etc.PCM Embedded (Protection from overcharging, discharge, and excess current)
Compatible Products

Controller : CM-510, CM-530, CM-700

Charger : LIPO Battery Charger LBC-10


Cannot be used with CM-100, CM-5, and CM-2+.

Storage Precautions

Do NOT charge the battery when the battery is connected to the robot or charger.

When storing away the battery for a long time, make sure the battery life is somewhere around 50%.

Do not place batteries in a place exposed to direct sunlight (between 0~45 degrees).

Do not store batteries with metal objects such as coins, keys, or jewelry.

Do not drop or give impact.

Do not apply water or any other liquid on the battery.

 

※ The warranty of LIPO 11.1V Battery Set LBS-10 is 6 months.

Caution

Not be charged through the robot, must be charged through the dedicated charger (LBC-10).

Do not drop the battery or shock it.

Do not operate the product during charging.

Do not heat the rechargeable battery or contact with fire, water, and other liquids.

Do not place the battery in a microwave oven, washing machine or dryer.

Damaged rechargeable batteries should not be used. (Swelling, deformed, damaged appearance, etc.)

Do not short-circuit the rechargeable battery anode and cathode.

Do not disassemble the rechargeable battery.

Before charging the rechargeable battery, make sure it is connected to the correct polarity and charge it.

Do not charge the rechargeable battery when it is hot.

Do not connect the rechargeable battery to the controller when not using the rechargeable battery.

Do not charge the rechargeable battery while it is connected to the controller.



1. All international orders are processed via DHL from KOREA (not USA) unless otherwise requested.
2. Orders are normally processed within a 2 week time period. A lead time is applicable for certain items. (Normally ships out within 3 working days when in stock).
3. If multiple orders are placed on the same day, they will be shipped in the same package, unless requested to ship separately by order. If an error is discovered in your order that requires change or cancellation, please contact us immediately. We will not be held responsible for any costs that may arise due to your negligence.
4. Please note that destination charges (import tax, customs duty, etc.) are not included in the shipping charges. We will not be able to calculate or pre-pay this fee for you.
5. If an order is placed and the payment is not settled within 14 days, it will automatically be cancelled. If necessary, please re-place the order and make the payment in a timely manner.
6. We recommend you to insure your orders to avoid lost or damaged shipments which is 1% from the total invoice value. We will not be held responsible for lost or damaged shipments.
1. If you are not completely satisfied with your order you may return it within 14 days from your shipment date for an exchange or refund. However, all non-defective products must be in their original packaging, and un-opened new condition. We will not be held responsible for return shipping charges.
All returns must go through the RMA process prior to being sent back to us.
Please note, we will not make any exchanges or repair unless WE HAVE ISSUED YOU AN RMA#.
Please check warranty.
2. Returned packages must include an RMA number on the outside of the package, as well as a copy of your printed invoice.
If you do not have your invoice, please include your name, address and phone number, so we may contact you regarding any questions we may have.
We have the right to refuse your shipment if we have not issued a RMA nubmer.
3. All returned items must be in there original package state. We are not responsible for damage to the print-head or circuitry as a result of improper handling, storage, or misuse.
When removing protective tape and devices please be sure not to damage these areas.
4. Requests for replacement or refunds will not be granted until your returned packages have been received.
5. Please allow up to 14 business days to process your refund from the time it reaches our warehouse, if you need an immediate replacement, we recommend that you place a new order and request a refund of the original order separately. We will not be held responsible for cancellatioin fees.
6. When returning any items, please confirm return address and keep note of the tracking number to avoid losing shipments.
We will not be held responsible for lost items.
7. We reserve the right to deny credit or replacements and charge the customer for parts and labor if the product returned are deemed satisfactory or non-defective.
8. We are not responsible for customer shipping costs to return non-defective or incorrectly ordered products.
9. Customers must obtain a Return Material Authorization('RMA') number by contacting Customer Service at contactus2@robotis.com. Returned products should be informed in advance before being returned.