/Hello,
I was studying how to use the ax-12a motors and found two contradictory pieces of information.
In the e-manual, (https://emanual.robotis.com/docs/en/dxl/ax/ax-12a/) the input voltage is said to be 9~12V. But in the ax-12 user´s manual (https://www.trossenrobotics.com/images/productdownloads/AX-12(English).pdf) it says that the intput voltage should be in between 7~10V.
Is this beacause the manual is outdated and references the old ax-12 model?
If so, why did the input voltage changed? Is it safe to use a 12V source for the ax-12a model? Are there any other changes you think i should take into consideration?
If no, which manual do i use as a reference for my build? Is 12V to much for the ax-12a model?
Thanks in advance,
Santiago
|
|
2021-05-19 08:58:21 |
| BearWitness | |
Probably best answered by someone from Robotis (and/or maybe Trossen Robotics).
These days I always go to Robotis Emanaul : https://emanual.robotis.com/docs/en/dxl/ax/ax-12a/
And yes you can use 12v with these. A simple hint on this, is if you buy a Trossen Robotics kit like:
https://www.trossenrobotics.com/phantomx-ax-hexapod.aspx
You will see they typically come with a 12v wall wart as well as a 3S Lipo which as about 11.1v up to
maybe 12.6v ...
|
|
2021-05-19 22:30:01 |
| kurteck | |
I think you were reading the product manual on the initial stage when the AX series was released. (2004)
Please reference the e-manual if you are using the latest version of AX-12A.
|
|
2021-05-20 13:58:42 |
| davidpark | |
Hi Santiago,
It is always safer to stick to the official documentation from the manufacturer.
AX series can run off of 12V, and the recommended voltage is 11.1V.
Thank you.
|
|
2021-05-24 13:56:02 |
| willson | |
|
|
2021-05-26 08:19:18 |
| BearWitness | |