...
POST No. 2408084
MX106-T Recovery failed
2021-10-12 15:48:35 2408057

For mx106-t steering gear, the protocol used is 2.0. When searching the steering gear with the software dynamixelwizard2, it cannot be found. When repairing the firmware, Dynamixelwizard2 does not respond during the repair process.

The R + Manager software can be used to search, control the LED and control the position rotation. The firmware cannot be repaired.

Then re use the Dynamixelwizard2 to search the steering gear. It can be found and controlled by the 2.0 protocol. It can't be repaired when repairing the firmware.

Cannot use 1.0 protocol

2021-10-12 15:48:35
2408057
2021-10-14 15:21:30 Will Son

Hi,


Thank you for your inquiry.

When configuring and testing DYNAMIXEL with ROBOTIS software, please use the official U2D2 or USB2DYNAMIXEL as our software is optimized and tested with these communication interface.

We cannot guarantee the compatibility with third party communication interface products and the ROBOTIS official software.


Thank you.

comment
2021-10-25 10:38:29 2408057
We also use the official ROBOTIS U2D2 or USB2DYNAMIXEL test, the phenomenon is the same. What is the reason for this?
thanks again
2021-10-25 10:38:29
2408057
2021-10-14 15:21:30
willson
2021-10-25 10:57:10 kay880


 

2021-10-25 10:57:10
2408057
2022-03-04 12:30:40 Patorn

I got same problem. It's because of wiring.


First, I use jumper wire connect with dynamixel's connector(as in picture). Motor could drive but recovery fail in some motor (Bootloader error).

After many tried, I try serious wiring with all male-female connector and plumbing wiring. Recovery is complete.


Then, I guess that jumper wire isn't fit well for dynamixel's connector (even though it feel so fit). It's not stable connection enough to run firmware (just drive motor or connect to Wizard is not problem).

 Even though, other motor is work, it might cause "Lucky" that at that time connection wasn't lost. Then, You should try serious wiring.


Hope this help.


 

2022-03-04 12:30:40
patorn.d
2022-06-24 03:22:10 noompang

pg slot สูตรลับ เทคนิคหรือสูตรลับแนวทางการเล่นสล็อต มีความง่ายๆ ไม่สลับซับซ้อน จาก pg slot สูตรลับ มีวิธีการเล่นที่มีระบบระเบียบแบบแผน พีจีสล็อต การเล่นเกมสล็อตให้สนุก นั้นต้องเล่นด้วยเงินจริง 

2022-06-24 03:22:10
noompang