When the AX-18A steering gear is in the position mode, the position information is not fed back. The steering gear cannot reach the specified position according to the command, but is rotating all the time. Try to repair the firmware to solve the problem, but the LED is always on after successfully repairing the firmware. The corresponding information cannot be found when using dynamixelwizard2 to find the steering gear. When using dynamixelwizard2 to repair the firmware, dynamixelwizard2 does not respond during the repair process.
|
|
2021-10-12 15:51:23 |
| 2408057 | |
Hi,
Leaving the third party serial-USB interface aside, I see that the LED of ID 10 AX DYNAMIXEL is turned on all the time, which means it doesn't have a proper firmware.
This could be caused by unsuccessful firmware recovery or corruption of the firmware.
Firmware recovery should be performed, but as I mentioned in the previous thread, it is recommended to use either U2D2 or USB2DYNAMIXEL when configuring DYNAMIXEL with ROBOTIS software.
Thank you.
|
|
2021-10-14 15:30:03 |
| willson | |
Thanks