...
POST No. 2408099
XM430-350R MX-64 bricked probably after firmware upgrade
2021-12-06 14:44:02 mrobotics

9 XM-430-350 R and 1 MX-64, they all got bricked. (all were in daisy chain)

Now none of the servos are getting detected and even the red light doesn't flash when first connected to power source/u2d2.

Connection cables, ports and U2D2 are perfectly fine as they are working with the other new servos that I have.


Any way to recover these servos?

2021-12-06 14:44:02
mrobotics
2021-12-13 10:11:58 Will Son

Hi,


I'm sorry about delayed response.


If the LED on DYNAMIXEL does not blink when powered, the firmware could be corrupted.

Please connect only one(1) DYNAMIXEL at a time and try the firmware recovery via DYNAMIXEL Wizard 2.0.


Thank you.

2021-12-13 10:11:58
willson
2021-12-23 15:51:46 bhuvnesh

Thank you very much Willson,
I was able to recover all the servos after firmware recovery.


Thank you.

2021-12-23 15:51:46
mrobotics
2022-02-24 14:19:57 Patorn

I get same problem(MX-106). I have tried to reinstall firmware, but 'Bootloader Error' occur. Could you have any suggest?

(It's working with the other mx-106 I have.)


 

2022-02-24 14:19:57
Patorn