I'm very glad that your company has new products on the market, especially the increase of small steering gear. I'm very excited,
However, an abnormal phenomenon occurred when we tested a small steering gear (xc330-t288-t), We use example / proctol2 of Dynamix SDK o / bulk_ Read_ Write. C program tests two steering gears (xc330-t288-t) to control the lights and control positions respectively, but they are stuck. What do you think is the reason?
Thank you again
|
|
2021-12-30 17:02:26 |
| 2408057 | |
Hi,
Have you modified the control table address definitions in the example code for the XC330?
The default example is written for PRO series which will not work for XC330.
For example,
Also, the Min, Max position value should be adjusted for XC330.
Please refer to the eManual below to find out the Control Table information and the valid range of value.
https://emanual.robotis.com/docs/en/dxl/x/xc330-t288/#control-table
Thanks!
|
|
|
||||
|
|
2022-01-03 17:41:03 |
| willson | |
Hello
Yes, you're right. We did find this parameter wrong at the beginning. This also gives you a suggestion. The SDK can form different folders according to different steering gears.
However, the solution you mentioned is not the problem. If you take a closer look at the screenshot I sent, it is normal when we test other demos (such as ping readwrite), except bulk_ There is a bug in readwrite. I suggest you try it yourself?
Thank you again
|
|
2022-01-04 13:50:54 |
| 2408057 | |
pg-slot.game เว็บ ปั่นสล็อต ออนไลน์ คุณภาพได้เงินจริง 100 % สามารถเล่นได้ตลอด 24 ชั่วโมง เล่นง่าย ได้เงินไว เล่นได้บนมือถือ
|
|
2022-06-24 00:46:46 |
| danny444 | |