...
POST No. 21000
DX117
2007-09-18 16:17:00
Dear Sir,

I'm Yu Tamai, a student of Ritsumeikan University.

We use DX117 and USBto485.

We got an error message from our system as follows:

ERROR_RCV_TMOUT

We have already checked the USBto485.
But we could'nt solve this problem.

And we could use the DXCONF.exe but our system has no response.

Could you give me any advice or comment?


Sincerely yours,
Yu Tamai.
2007-09-18 16:17:00
2008-08-28 16:03:00 ROBOTIS
Dear Yu Tamai san.Thank you for your question.With the below information, it is hard to know how the situation is.Please give me more information as in environment-wise.Then. I will be able to assist you.Thank you.
2008-08-28 16:03:00
robotis
2008-08-28 16:03:00 ROBOTIS
Dear Sir,Thank you for your rapid reply.I show you information of our environment as follows:1.hardware environment i. PC Celeron 2.8GHz memory 448MB (WindowsXP) ii. USBto485 and CM2 are used to connect PC and the hand.2.condition of the problem We can use DXCONF.exe and Robot_Terminal.v0.91.exe regularly. But neither Packet_control.exe nor Robot_control.exe work well. In our program, the function DXL_open() succeeded. And DXL_robot_create() returns 1. (It seems to work well.) But the following DXL_robot_get_info() returns FALSE. (DXL_actuator_get_info() returns 37(ERROR_RCV_TMOUT) if it is called after DXL_robot_create().) Since DXCONF.exe works well, the electoric connection between PC and the hand seems to work well.Do you have any advice?Sincerely yours,Yu Tamai
2008-08-28 16:03:00
robotis