Hi, my robot is Bioloid Robotis STEM. I assembled the car robot but few days ago it began failed or just not working. First of all, I have to solve the battery beep. I read round here that it is because of the controller (CM-530, in my case) but, as I can notice, it works thanks to the 1,5v batteries, and it has all of them!
I checked if they were low voltage but they don't. And also, I saw near the power ON/OFF bottom, a led where you can read '12V DC', but this is too much voltage for a led, isn't it? What can I do? Am I wrong with the controller? Thanks.
|
|
2021-01-15 04:40:47 |
| Fernandez | |
Hi,
Thank you for your inquiry.
Could you give us more information about the example you assembled?
In order to run the example properly, you need to upload the TASK file on your CM-530.
Please select the example you assembled in the manual, and download the Practical Phase task code, then upload it to CM-530 using either Task 3.0 or Task 2.0
Thank you.
|
|
2021-01-19 11:05:34 |
| willson | |
Hi, I assembled the first one: 1. Sequence Racer . I tried this morning uploading Task 3.0 again, just in case this problem was solved, but the annoying beep keep sounding when I press the start button. Could you tell me if it is possible attach a video with my robot and its beep in this text space? Thanks.
|
|
2021-06-23 20:35:03 |
| Fernandez | |