Hi,
I am using a combination of PRO series and MX Series all connected in Daisy chain.
I use Dynamixel Adapter to convert RS-485 to USB.
I referred to the following page.
I can move moter with kinetic.
But I want to move moter with melodic.
I get the following error when I run the hardware melodic with the same configuration as the kinetic configuration.
[ERROR] [1611035517.462351680]: [TxRxResult] Incorrect status packet!
[ERROR] [1611035517.462547520]: groupSyncRead getdata failed
[ERROR] [1611035517.462700224]: groupSyncRead getdata failed
[ERROR] [1611035517.462805952]: groupSyncRead getdata failed
I restart Dynamixel by error every time.
This error is known that this is due to the connection from MX to PRO and the power pin is not connected.
But I don't know how to avoid error.
I setup melodic is new seting.
I did the above.
Kindly help me, I got stuck here.
Thanks.
|
|
2021-01-19 16:04:29 |
| kuroikei | |
I have confirmed that this setup gives the same error in Kinetic.
|
|
2021-01-19 16:06:10 |
| kuroikei | |
Hi... I like the OpenManipulator-X and TurtleBot combination. For starters their combo is based on TurtleBot3 and not 2. And I like the OpenCR ness. But then i lose what Trossen brings to the table. And vice versa. If i go with the LocoBot i lose what Robotis brings to the table.
|
|
2021-01-29 01:39:18 |
| KaraPelosi | |