Hi,
I am currently working on a robotic arm. I am using these:
The two XM540-W270 are on the same joint. One of them is in slave mode. The other motors control the other joints. I therefore have a 5 degree of freedom robotic arm (you get the picture?).
The baudrate of each motor is at 4 000 000 bps. The usb port (COM) is set at 9600 bps and has latency time of 1 ms.
My problems are the following:
When I scan my motors on Dynamixel Wizard, the software doesn’t always detect 6 motors. Would you know why? When it happens, I just scan it again until it detects 6 motors.
I always get the Time Out pop up (as shown on the picture):
As for the connection setup, see picture below:
The Rx Tx wire are all in series between the different motors.
Thanks a lot!
|
|
2021-05-20 21:53:56 |
| Xavixav | |
Please refer to the redundant issue thread below.
https://community.robotsource.org/t/time-out-pop-up-in-dynamixel-wizard/2054/3
|
|
2021-05-25 13:16:55 |
| willson | |