Hello, I am trying to setup the Turtlebot3 Burger (Raspberry Pi 4 - 4GB) with the ROS Melodic image provided in the manual, though I am not able to login as the connected USB keyboard is not working and seems not even powered as none of the LEDs is on.
The problem must be a software issue because:
- I read that there are quite a few problems concerning power supply with keyboards though I use a Logitech K120 which is on the list of keyboards that work and a colleague also used this exact keyboard with another Raspberry Pi. On my Laptop the keyboard is working as well.
- I tried flashing Ubuntu 21.10 on the same Raspberry Pi and the keyboard works without problems.
- I get a "Failed to start Load Kernel Modules" during startup
- LIDAR is running on same USB port when connected
What I tried:
- I tried connecting the keyboard to all USB ports and rebooting - I tried flashing the image multiple times
- I also tried adding "total_mem=3072" to the usercfg.txt as suggested here: https://ubuntu.com/blog/roadmap-for-off ... berry-pi-4 (Even though in the Ubuntu image that I flash the file is not in /boot/firmware/ as described but in a system_boot partition)
Does any of you have another idea what could be the problem and how I can get it to work? I am thankful for any ideas!
|
|
2021-11-30 17:13:24 |
| jherzfel | |
Hi,
If you have other USB keyboards or wireless keyboards with a USB dongle, I'd recommend try those as this could be an issue of the compatibility between Raspberry Pi and the specific keyboard.
Also, if possible, please use a USB dongle as some wired keyboards may require more power from the USB port.
Thank you.
|
|
2021-12-01 10:42:42 |
| willson | |
เครดิตฟรี คืนยอดเสีย โปรโมชั่น ดีๆที่เราพร้อมจะแจกจะ ช่วยทำให้การเดิมพันของคุณนั้น เล่นได้มากยิ่งขึ้นกว่าเดิม พีจี ยิ่งเล่นยิ่งรวยใน การเล่นเกมกับ บรรดาเว็บทั้งหลายนั้น
|
|
2022-06-25 16:01:06 |
| Suwithwat | |