...

Item Information

X540-270 Gear/Bearing Set

Gearset for X540-270, including bearings and grease

상품 선택옵션 0 개, 추가옵션 0 개

SKU 903-0285-000
Manufacturer ROBOTIS
Origin Korea
Currency USD
Price $ 131.40

선택된 옵션

  • Quantity

상품 기본설명

Features

Gear set for Dynamixel XH540/XM540 – Gear Ratio: 270 : 1

 

Can be replaced directly when existing gears are worn out.

 

Made with metal and specially coated to strengthen endurance and durability of abrasion.

 

Exclusive magnet for non-contact absolute encoder is attached to the wheel gear.

 

Package Components
X540 Gear #1 (for 270)1
X540 Gear #2 (for 270)1
X540 Gear #31
X540 Wheel Gear1
Grease1
Calibration Adaptor (for X540)1
Ball Bearing2
Gear Replacement Procedure

X430 and X540 applied in the same way

Gear Calibration Procedure
Compatible Products


DYNAMIXELX540-270 Gear SetX540-150 Gear Set
XH540-W270-RO
XH540-W270-TO
XH540-W150-R
O
XH540-W150-T
O
XH540-V270-RO
XH540-V150-R
O
XM540-W270-RO
XM540-W270-TO
XM540-W150-R
O
XM540-W150-T
O
Caution

Two ball bearings are used for the wheel gears.

The bearing of the bottom wheel gear is connected when shipped.

When replacing the gear, assemble after connecting the top wheel gear.


 

It is possible to recycle the used bearings, but it is recommended to use new ones because of the performance degradation due to abrasion, debris, etc.


 

Since Dynamixel X series use non-contact magnetic encoders, you will have to calibrate to align the initial position after gear replacement.


 

Use R+Manager2.0 to process the calibration along with the calibration adapter.

 

 

These are not compatible with DX/RX/MX series.

1. All international orders are processed via DHL from KOREA (not USA) unless otherwise requested.
2. Orders are normally processed within a 2 week time period. A lead time is applicable for certain items. (Normally ships out within 3 working days when in stock).
3. If multiple orders are placed on the same day, they will be shipped in the same package, unless requested to ship separately by order. If an error is discovered in your order that requires change or cancellation, please contact us immediately. We will not be held responsible for any costs that may arise due to your negligence.
4. Please note that destination charges (import tax, customs duty, etc.) are not included in the shipping charges. We will not be able to calculate or pre-pay this fee for you.
5. If an order is placed and the payment is not settled within 14 days, it will automatically be cancelled. If necessary, please re-place the order and make the payment in a timely manner.
6. We recommend you to insure your orders to avoid lost or damaged shipments which is 1% from the total invoice value. We will not be held responsible for lost or damaged shipments.
1. If you are not completely satisfied with your order you may return it within 14 days from your shipment date for an exchange or refund. However, all non-defective products must be in their original packaging, and un-opened new condition. We will not be held responsible for return shipping charges.
All returns must go through the RMA process prior to being sent back to us.
Please note, we will not make any exchanges or repair unless WE HAVE ISSUED YOU AN RMA#.
Please check warranty.
2. Returned packages must include an RMA number on the outside of the package, as well as a copy of your printed invoice.
If you do not have your invoice, please include your name, address and phone number, so we may contact you regarding any questions we may have.
We have the right to refuse your shipment if we have not issued a RMA nubmer.
3. All returned items must be in there original package state. We are not responsible for damage to the print-head or circuitry as a result of improper handling, storage, or misuse.
When removing protective tape and devices please be sure not to damage these areas.
4. Requests for replacement or refunds will not be granted until your returned packages have been received.
5. Please allow up to 14 business days to process your refund from the time it reaches our warehouse, if you need an immediate replacement, we recommend that you place a new order and request a refund of the original order separately. We will not be held responsible for cancellatioin fees.
6. When returning any items, please confirm return address and keep note of the tracking number to avoid losing shipments.
We will not be held responsible for lost items.
7. We reserve the right to deny credit or replacements and charge the customer for parts and labor if the product returned are deemed satisfactory or non-defective.
8. We are not responsible for customer shipping costs to return non-defective or incorrectly ordered products.
9. Customers must obtain a Return Material Authorization('RMA') number by contacting Customer Service at contactus2@robotis.com. Returned products should be informed in advance before being returned.
  • 12.0V / 10.6Nm / 30.00rpm / Coreless / Metal ...
    $ 429.90
    Lead Time :40 days
  • 12.0V / 10.6Nm / 30.00rpm / Coreless / Metal ...
    $ 419.90
    Lead Time :40 days
  • 12.0V / 9.90Nm / 39.00rpm / Coreless(Maxon) /...
    $ 549.90
    Lead Time :50 days
  • 12.0V / 9.90Nm / 39.00rpm / Coreless(Maxon) /...
    $ 539.90
    Lead Time :40 days
  • 24.0V / 9.20Nm / 34.00rpm / Coreless(Maxon) /...
    $ 549.90
    Lead Time :40 days
  • 12.0V / 9.90Nm / 39.00rpm / Maxon / Long Life...
    $ 769.90
    Lead Time :60 days